Carrier® High Efficiency Heat Pump with Greenspeed™ Intelligence Named One of the "Hot 50 Products of 2012" by GreenBuilder Magazine

Indianapolis, Indiana, May 17, 2012 – The Carrier® Infinity® 20 heat pump with Greenspeed™ intelligence was recently voted one of “The Hot 50 Products of 2012” by GreenBuilder magazine, a leading North American residential building industry publication. The GreenBuilder panel of judges selected the Carrier heat pump product based on its overall impact, innovation and reliability. Carrier, the world’s leader in high technology heating, air-conditioning and refrigeration solutions, is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp. (NYSE: UTX).

GreenBuilder: The Hot 50 Products 2012

Introduced in 2011, the Infinity heat pump with Greenspeed intelligence has an HSPF (Heating Seasonal Performance Factor) efficiency rating up to 13, making it the highest heating efficiency ducted, air source heat pump on the market. The Infinity heat pump delivers up to 69 percent higher heating efficiency in the three-ton size.

“Carrier is proud that the Infinity 20 heat pump with Greenspeed intelligence has been named one of ‘The Hot 50 Products of 2012’ by GreenBuilder magazine” said Matt Nuijens, Carrier brand manager. “As a company committed to sustainability, Carrier continually improves on the performance and efficiency of its products. It is a tremendous honor to have this new heat pump included as one of the 50 building products that raise the bar a little higher in the industry.”

The Infinity 20 heat pump with Greenspeed intelligence was one of four HVAC (heating, ventilation and air conditioning) products to receive the “Hot 50 Products of 2012” designation from GreenBuilder magazine.

“One of the many innovative features of the Infinity 20 heat pump is its ability to provide warmer air at the register when outdoor temperatures fall into the teens,” said Rob Lambert, Carrier product manager and application engineer. “Under similar conditions, standard heat pumps may deliver cooler air at the register when outdoor temperatures decline. The Infinity 20 heat pump is one of the highest efficiency air source heat pumps built with consumer comfort in mind.”

When installed as part of a complete Infinity system, the new heat pump adjusts its output within a range of 40 to 100 percent of capacity to match the heating or cooling requirements of a home. This innovation is made possible by pairing the superior communication ability of Carrier Greenspeed intelligence with a Copeland Scroll® variable -speed compressor from Emerson Climate Technologies, optimized specifically for this heat pump.

With cooling efficiencies of up to 20.5 SEER and variable-speed compressor technology, this new heat pump is also ideal for superior cooling and dehumidification in regions with warmer temperatures and high humidity.

For more information on the Infinity 20 heat pump with Greenspeed intelligence or additional Carrier products and services, call 1-800-CARRIER or go to www.carrier.com.

About Carrier

Carrier is the world’s leader in high technology heating, air-conditioning and refrigeration solutions. Carrier experts provide sustainable solutions, integrating energy-efficient products, building controls, and energy services for residential, commercial, retail, transport and foodservice customers. Founded by the inventor of modern air conditioning, Carrier improves the world around us through engineered innovation and environmental stewardship. Carrier is a part of UTC Climate, Controls & Security, a unit of United Technologies Corp., a leading provider to the aerospace and building systems industries worldwide. Visit www.carrier.com for more information.

Important Message!

We have recently updated and moved the Carrier site.
Information on this page is no longer being updated.
Click here to be redirected to the new Carrier Home Comfort site.