Ductless Split Systems

 

What is a ductless system?

Not every room has ductwork for heating or cooling. Sometimes providing adequate comfort in commonly used spaces means wasting energy elsewhere. Usually these spaces lack ductwork; however, hot or cold spots can exist even in rooms with ductwork.

CarrierĀ® ductless systems are innovative heating and cooling solutions that make sure non-ducted spaces are as comfortable as any ducted space, so you can expand your living and work areas. These high-efficiency systems can also help you save money by helping to keep your most-used rooms optimally comfortable, so that even if you have ductwork, you can potentially spend less on heating and cooling costs for the rest of the residential or commercial space.*

High-efficiency Toshiba-Carrier high-wall systems use inverter technology to consistently deliver precision heating and cooling while only using the energy that is needed at any given time. No blasting of hot or cold air. And with cooling efficiencies as high as 23 SEER, Toshiba-Carrier ductless systems are some of the most energy-efficient ways to cool a space.

Ace Air logo

Targeted comfort systems are generally dedicated to a single room, though multiple-unit options exist and can be placed throughout a home if the need is there. Ductless systems are often used to improve the energy use fully ducted homes and businesses to take care of hot or cold spots, or to help improve the energy efficiency of the surrounding spaces. They can also be used in temperature-sensitive rooms where storage or data needs to be protected.

Your Carrier expert can help determine what is the best system for your situation and can have it installed within a few hours. High wall-mounted system installations require only a small hole through the wall to connect pipe from the indoor unit to the outdoor unit. Then it just takes an electrical connection outside and a few screws to mount the unit to the wall, and the installation is complete.

*not applicable to ducted zoned applications

Ace Air logo